|
ARD2
1.00 for Rev B. Hardware
Airbag Reference Demonstrator using MPC5604P
|
State used to send and receive data from demo GUI. More...
#include "derivative.h"#include "Compile_Options.h"#include "GUI_State.h"#include "SM.h"#include "SBC_AL.h"#include "CG147.h"#include "CG147_Diag.h"#include "Central_Accel_AL.h"#include "MMA68xx.h"#include "MMA68xx_Diag.h"#include "DSPI.h"#include "HAL.h"#include "MailScheduler.h"#include "Application_Globals.h"#include "MMA51xx.h"#include "SIU.h"#include "Labview.h"#include "IntcInterrupts.h"#include "Utils.h"#include "LIN_UART.h"#include <Limits.h>Functions | |
| uint32_t | u32fnStateGUI (void) |
| Demo mode GUI state takes over diagnostics state. | |
| void | vfnGUIStateFormatCurveData (uint16_t *au16LabviewData) |
| This function takes data from gau16RawAccels and formats it into a Labview-friendly format. | |
| uint32_t | u32fnGUISwitchCase (const uint8_t *pu8Cmd, uint8_t *pu8RawResponse, uint8_t *pu8Size, uint8_t *pu8TextResponse, uint8_t *pu8TextSize) |
| Used to select which command will be executed, based on the incoming message. | |
| uint32_t | u32fnGUISendResponseFrame (const uint8_t *pu8Cmd, const uint8_t *pu8RawResponse, const uint8_t *pu8Size, const uint8_t *pu8TextResponse, const uint8_t u8TextSize) |
| After the raw response is ready, this function formats it into the correct format and sends it over to the GUI. | |
| void | vfnGUISBCCapTests (uint8_t *pu8Size, uint8_t *pu8RawResponse, uint8_t u8ERx, uint8_t u8Test) |
| Performs Cap tests as requested by the GUI. | |
| void | vfnGUISBCLeakageTests (const uint8_t cu8Side, const uint8_t cu8Squib, const uint8_t cu8LeakageType, uint8_t *pu8Result) |
| Performs a specific leakage or resistance tests (squibs). | |
| void | vfnGUICheckSatellites (const uint16_t *pu16Mask, uint8_t *pu8Result) |
| Verifies that satellites have started up correctly by restarting them. | |
| void | vfnVerifyValidityOfCmd (const uint8_t *pu8Cmd, const GUICmdString_t *ptValidCmd, const uint16_t u16TableSize, uint8_t *pu8Result) |
| Verifies that a given command is in the list of approved commands (catGUIValidCommands). This function is directly linked to command '1'. | |
| void | vfnGUISatAndSquibState (const uint8_t u8Mode, const uint16_t cu16Step) |
| Used to send to GUI a verbose list of active satellites and squibs Due to time constrains, this function is broken into n subsections or threads. | |
State used to send and receive data from demo GUI.
Copyright (C) 2011 Freescale Semiconductor Freescale Confidential Proprietary
History:
| uint32_t u32fnGUISendResponseFrame | ( | const uint8_t * | pu8Cmd, |
| const uint8_t * | pu8RawResponse, | ||
| const uint8_t * | pu8Size, | ||
| const uint8_t * | pu8TextResponse, | ||
| const uint8_t | u8TextSize | ||
| ) |
After the raw response is ready, this function formats it into the correct format and sends it over to the GUI.
| pu8Cmd,: | pointer to the command and arguments used for the previous response. |
| pu8RawResponse,: | Pointer to memory location where the response is to be stored. First element must be either '00' or '01' for passed or failed, and the next locations should contain data. |
| pu8Size,: | Pointer to location where the size of the raw response is stored. |
| pu8TextResponse,: | Pointer to memory location where a text message is stored. It will be sent as status. |
| u8TextSize,: | Size for TextResponse. |
| uint32_t u32fnGUISwitchCase | ( | const uint8_t * | pu8Cmd, |
| uint8_t * | pu8RawResponse, | ||
| uint8_t * | pu8Size, | ||
| uint8_t * | pu8TextResponse, | ||
| uint8_t * | pu8TextSize | ||
| ) |
Used to select which command will be executed, based on the incoming message.
| pu8Cmd,: | Pointer to command and arguments structure. |
| pu8RawResponse,: | Pointer to memory location where the response is to be stored. First element must be either '01' or '00' for passed or failed, and the next locations should contain data. |
| pu8Size,: | Pointer to location where the size of the raw response will be stored. |
| pu8TextResponse,: | Pointer to memory location where a text message will be stored to be sent to GUI as status. |
| pu8TextSize,: | Pointer to location where the size for the status message size will be stored. |
| uint32_t u32fnStateGUI | ( | void | ) |
Demo mode GUI state takes over diagnostics state.
| Void. |
| void vfnGUICheckSatellites | ( | const uint16_t * | pu16Mask, |
| uint8_t * | pu8Result | ||
| ) |
Verifies that satellites have started up correctly by restarting them.
| pu16Mask,: | Pointer to mask list with all satellites to be tested. |
| pu8Result,: | Pointer to memory location where the response is to be stored. First element must be either TRUE or CLEAR for passed or failed, and the next locations should contain data. |
| void vfnGUISatAndSquibState | ( | const uint8_t | u8Mode, |
| const uint16_t | cu16Step | ||
| ) |
Used to send to GUI a verbose list of active satellites and squibs Due to time constrains, this function is broken into n subsections or threads.
| u8Mode,: | Selects between parallel or serial transfer of info. |
| cu16Step,: | Execution step. |
| void vfnGUISBCCapTests | ( | uint8_t * | pu8Size, |
| uint8_t * | pu8RawResponse, | ||
| uint8_t | u8ERx, | ||
| uint8_t | u8Test | ||
| ) |
Performs Cap tests as requested by the GUI.
| pu8Size,: | Pointer to location where the size of the raw response is stored. |
| pu8RawResponse,: | Pointer to memory location where the response is to be stored. First element must be either '00' or '01' for passed or failed, and the next locations should contain data. |
| u8ERx,: | Defines which ERx to perform the test on. |
| u8Test,: | Test index according to cau8SBCTests. |
| void vfnGUISBCLeakageTests | ( | const uint8_t | cu8Side, |
| const uint8_t | cu8Squib, | ||
| const uint8_t | cu8LeakageType, | ||
| uint8_t * | pu8Result | ||
| ) |
Performs a specific leakage or resistance tests (squibs).
| cu8Side,: | low (TRUE) or high (CLEAR) side |
| cu8Squib,: | Any valid squib index, from 0 - 11. |
| cu8LeakageType,: | Low leakage (TRUE) or high leakage (CLEAR). |
| pu8Result,: | Pointer to memory location where the response is to be stored. First element must be either TRUE or CLEAR for passed or failed, and the next locations should contain data. |
| void vfnGUIStateFormatCurveData | ( | uint16_t * | au16LabviewData | ) |
This function takes data from gau16RawAccels and formats it into a Labview-friendly format.
| au16LabviewData,: | Pointer to the location where the Labview array should be placed. |
| void vfnVerifyValidityOfCmd | ( | const uint8_t * | pu8Cmd, |
| const GUICmdString_t * | ptValidCmd, | ||
| const uint16_t | u16TableSize, | ||
| uint8_t * | pu8Result | ||
| ) |
Verifies that a given command is in the list of approved commands (catGUIValidCommands). This function is directly linked to command '1'.
| pu8Cmd,: | Pointer to commands and arguments. |
| ptValidCmd,: | Pointer to the list of valid commands and arguments. |
| u16TableSize,: | Number of elements in ptValidCmd |
| pu8Result,: | Pointer to memory location where the response is to be stored. First element must be either TRUE or CLEAR for passed or failed. |